STM32Cube for Agentic AI Installer ¶
The
STM32Cube for Agentic AI installer
is the command-line entry point for setting up and
maintaining the STM32Cube Agentic Context toolkit on your machine and in your projects. Use
cube
agentic-ai
for installer commands. Context bundle names follow the
cube-agentic-ai-<connector>
pattern.
This reference explains command syntax, defaults, deployment state, and project maintenance. For a first installation, use the installation guide in SEE ALSO. For context capabilities and typical development requests, use the STM32Cube for Agentic AI documentation in SEE ALSO.
The reference is published online and is also included in the installer
bundle. Run
cube
agentic-ai
get-user-manual
--format
html
to open the
bundled HTML manual, or use
--format
tldr
for a concise command summary.
The bundled manual describes the installed installer version. The online
manual can describe a newer release.
It gives you a stable command set to:
Set up the toolkit in one command (
setup): install on the machine, resolve what the contexts need, and deploy into a project.Diagnose what the installed contexts need to work, and fix it (
doctor).Install STM32Cube Agentic Context bundles on your machine.
Deploy them into a project folder, wiring skills, agents, instructions, prompts, and MCP servers to your agentic AI system.
Lock the exact versions used in a project so the setup is reproducible.
Inspect what is installed and what is deployed at any time.
Command results use machine-readable JSON, so both human operators and agentic AI systems can drive the same workflow. Interactive commands also print prompts. Help and version requests print text.
Scope ¶
The installer covers:
|
Area |
What the installer does |
|---|---|
|
Machine setup |
Install context bundles via the
|
|
Requirements |
Check what contexts need (
|
|
Tool dependencies |
When a context requires a Cube tool, the
|
|
Project deployment |
Deploy STM32Cube Agentic Context files into your project folder |
|
Target wiring |
Place files in the right location for your IDE and agentic AI system, or use the portable
|
|
Version locking |
Record exact context and tool dependency versions so projects are reproducible |
|
Routing catalog |
Generate a Markdown catalog from services declared by contexts deployed to the project |
Contexts use consistent project-file ownership, so the installer can track the files it deploys
for later updates and removal. When a context requires a Cube tool, the
cube
bundle
manager installs that tool automatically.
The installer does not:
Install VS Code extensions without authorization:
setup --install-vscode-extensionsinstalls declared extensions, anddoctor --fix --vscode-profile "<name>"installs missing declared extension dependencies only in that explicitly named, existing profile. Other extension checks report commands to run. The commandssetupanddoctor --fixalso run a bundle’s declared Python-package installation. Neither installs Python itself.Maintain a separate catalog of tools — tool lifecycle is the responsibility of the
cubebundle manager via context dependencies.Modify IDE settings beyond the documented project wiring and explicitly authorized extension installation.
Quick orientation ¶
Concepts — concise conceptual model: context bundle vs tool bundle, automatic tool dependencies, versioning, scope boundaries, lock files, and routing catalog.
Prerequisites — what must be installed on your machine before running any command.
Commands reference — full syntax, options, and defaults for all commands.
Target selection — how
--ideand--agentic-systeminteract, with the common deployment patterns.Lock files — how the installer records deployed versions and service selections, and how to reproduce a project environment.
Project housekeeping — strategy guide for evolving deployments with add/remove/deploy flows.
Usage — annotated command sequences for the most common workflows.
Troubleshooting — error codes, their meaning, and the next action to take.
Routing behavior ¶
Project commands use the
usage-router
mode by default. This mode generates the routing catalog
from services declared by the contexts deployed to the project. It does not arbitrate overlapping
context responsibilities. To opt in to overlap arbitration, pass
--routing-mode
usage-router-with-arbitration
to a project deployment command.